This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP9204: This is reference Design AC DC SMPS

Part Number: PMP9204

Heelo,

I have Design AC to DC Power Supply in my board. Please share me solution as per given below requirement-

1. Input Voltage - (85 to 264)VAC 

2. Output Voltage- 5VDC/1A (But I have design upto 2A) 

3.Voltage Accuracy- 1% to 2%

4.Power -5W/10W

5.Line Regulation- 1%%

6.Load Regulation- 1%

7.Ripple- 50 to 150mV

8.Efficiency-80 to 90%

9. Isolation- 4000VAC (Input to Output)

10.Protection- Over Current, Short Circuit, Over voltage and Temperature Protection

I have  select PMP9204. This is suitable design