Part Number: PMP9204
Reference Design Number- PMP9204 (85-265) VAC
- Can This Power Supply working input Voltage (75 to 275)VAC
What is min Ac Voltage is working with 1A Load
- I want to set output Voltage 5.1 or 5.2VDC. Which resistance value is change in Circuit?
- I want to set input under voltage and input over voltage limit. How will be set in circuit.
- Line and Load Variation
- I seen part number of transformer RLTI-1067 in BOM but there is no stock. Please suggest me any alternate part number of transformer.