This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010071: TIDA-010071

Part Number: TIDA-010071

We are writing this query w.r.t the Table.6 of TIDA-010071. According to the table for STATE-D the pilot high voltage need to be 3V for a resistance of 246Ohm, but as per our simulation observation we are getting voltage of 2.5V only. See could you please share the test data results and simulation results as well for the same for our understanding.

Thanks & Regards

Prasad

  • Hi Prasad,

    Thank you for your post.  I will take a look it this and see what test results/answer I can find on the State-D voltage potential on TIDA-010071.

    Best regards,

    Errol

  • Hello Prasad,

    I have looked into the standards and seeing if there is test data for this design.  Unfortunately since this is an old design we could not locate the testing data for this design for state D.  However,  I have looked in to the nominal values of the resistance simulated the different states and the nominal value for state D should be 270 ohms as shown below.  When changing the value we get 3.03V in simulation.

    I am also attaching the modified simulation file as well.

    Best regards,

    ErrolPilotSim_TLV1805.TSC