This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP22650: Recommended list of test equipment to validate the PMP22650 reference design.

Part Number: PMP22650

Hello,

We are planning to assemble the PMP22650 and have been reviewing the documentation avaialable.

The test report in the following link: https://www.ti.com/document-viewer/lit/html/TIDT249/GUID-8D2A5028-A724-480A-BEA4-5AD53E44E359#GUID-CCCD2933-BF9E-4525-A4DC-F02E47379022

Shows a list of required equipment for test: 

    • 240 VAC, 7 kW AC source

    • 250 V to 450 V, 6.6 kW DC load

    • 12 V, 2 A bias supply

    • Refrigerated recirculating chiller

Could you please recommend Manufacturers and part numbers for these equipment so that we work with a similar lab setup?

Thank you