This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSPICE-FOR-TI: Warning (ORCAP-2445): Model not found in the configured libraries.

Part Number: PSPICE-FOR-TI

I just built this simple circuit (below) but when I try to simulate it two warning signals appear. It says Warning (ORCAP-2445): Model X not found in the configured libraries. The thing here is I took these 2 parts (MUR150 AND IRF840) from the libraries that come with the software (diode.olb and irf.olb), respectively). I even put the pathway for each library on the configured libraries for the simulation file but I still can't make it work. See below screenshots of the circuit and the errors.

Is there any way to make this work?