This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power Control Circuit for Multiple PM Linear Generators

Other Parts Discussed in Thread: UCC28740, UCC28C53

How would one go about making a power control circuit to combine the waveforms of 2 linear generators, each with unique frequencies, amplitudes, and periods for each EMF pulse (the peaks have great variance, ranging from 50V to 120V)? Then deliver that generated power to a given load, such as a battery? What about if each generator consisted of a three phase system instead of a single phase? A circuit diagram for a general approach to this problem would be very much appreciated! Thanks!