Part Number: TIDA-020031
Customer is referring to both TIDA-020031 and SLUA560D
They have some questions about how max Duty cycle is selected.
SLUA560D use 70% as the max duty cycle in equation (4),
In design, use a center-tap transformer, which leads to a 21:1:1 transformer.
In TIDA-020031, use 'secondary duty max' as 90%. This design uses a current doubler on the secondary side.
- Eq (4) in SLUA560D and Eq(4) in TIDA-020031 similar other than "Dmax" and "Dsec_max".
- Can you explain the differences in "Dmax" and "Dsec_max"?
- How should we define Duty_max for our design?
- Eq(5) in TIDA-020031, How to define Vsec_min ?