I'm trying to use Pspice for TI to simulate the behaviour of LM61460-Q1 with different input capacitors.
The version of I'm using is:-
For the capacitors I downloaded the GCM.LIB file from the Murata website and then followed the "PSpice for TI: 3rd Party Model Import" video to create a symbol, assign pins and configure the .LIB file.
When I placed a component from this library Pspice for TI froze and Windows reported it as "Not Responding" for about 40 seconds.
Now any operation on that component (move, rotate, copy, paste, add wire, move wire etc.) causes another 40s of "Not Responding".
Adding further GCM capacitors also causes another 40s of "Not Responding".
Other operations on the schematic (including adding components from the Pspice libraries) does not cause "Not Responding".
The circuit does simulate but I may have to retire before I can draw the rest of the capacitors that I want to simulate.
I've attached a zip of the project including the Murata library files.
Please can you tell me how to avoid these "Not Responding" delays?