Good Morning,
I am working through the apps note for the TIDA-010242 and checking the calculations with a view to modifying or creating a similar design for a slightly modified version of 1275D.
I am currently looking at the SOA calcs in para 2.2.6 and I would like to ask a little about the numbers that are in the apps note.
I follow the concept of calculating the stress square pulse and I get the same values shown. When I get the SOA calcs I believe that the design is extrapolating from the SOA chart from the manufacturer.
Would you be able to explain how the 1 second and 10ms currents were extrapolated at the 50V line? By eye I would choose slightly different values, but I wondered if you were calculating them somehow?
If I use the values given in the notes then I get the same current at the 218ms square pulse model time, and at this point I'm not able to understand the power or time that is mentioned in this sentence:
"Plugging in the numbers for the IXTT88N30P results in an SOA of 15.7 A, meaning that the IXTT88N30P can handle 439.6 W for 252 ms. Which indicates this is more than enough for a 120-W system at
25°C."
Could you detail how these figures are calculated? I'm wondering if they are based on projecting the SOA current of 15.7A on the 50V line for the time, but the figures seem too accurate for a visual estimation.
Thanks in advance!