Dear Support,
I am trying to simulate a circuit with TINA including a BC337-25 transistor. I have had a lot a trouble in doing that and eventually I pinpointed the problem in the BC337-25 model available in TINA.
If you select the SPICE-BJT model, even if the beta forward is set at 347, the simulation gives @(Ic=10mA, Vce=5V) a bare beta of 80 (please see the file bc337-25_SPICE_BJT_Ic_Vce_Ib.TSCand run Ctrl-Alt.R)
If you select the HybridP model, the beta seems fine, yet the Vbe during transient simulation is definitely wrong.... (see the file bc337-25_HybridP_Ic_Vce_Ib.TSC
If you simulate the simplest possible amplifier with the SPICE-BJT model, you find a Vbe of 1.1V, which is fully wrong... see file CE_amplifier_Bc337_HybridP.TSC
Am I doing something wrong? I really appreciate your help and support. best, Alberto