Part Number: TIDA-00663
Other Parts Discussed in Thread: TDC7200
Hi,
I've been wrestling with the time calculation so far (minus vacation): the values of time1 stay now smaller than the values of time2!
Another observation is that the interrupt line of one TDC7200 is low (as it should) while the second interrupt is always high. I replaced both TDC's with no improvement.
I receive for both TDC's after a start/stop sequence a status of 0b00011001 as return which looks ok.
The SPI clock is 9.4 MHz and the clock for the TDC's is 16 MHz.
Anyone an idea where to start digging?
Thanks for helping on this.