Part Number: PSPICE-FOR-TI
Hi,
I wanted to compare simulation results from PSPICE for TI without giving any max. step size and giving a max step size in simulation settings.
but when I see results with max step size provided, It is showing huge noise. please see the below attached images.
with step size given in simulation settings:
Step size: 0.001e-6
with default max, step size: means no step size given in simulation settings.
As we can see in the results, if I do not provide any max. step size in settings it is giving me a good wave form. which one should I consider?
Please help me.
Thanks
Sai Kumar