Other Parts Discussed in Thread: SFRA,
Hello,
I have cleared Lab1 for the TTPL PFC.
As per the the section (3.1.2.5.2.3) of TIDUET7G, Lab 2 test, the expected result is given as 46V, 0.7Amp at 100 Ohms Load.
However on running the same code without any changes to the same board (just with changed Inductor with inductance value around 500uH at no load)
I am getting around 68V at the output with the following values and the TTPLPFC_DutyPU is also a little higher- 0.419(compared to 0.2625 in the screenshot of document)
Also according to the Boost equation, with 0.2625 duty, the output voltage should be around 40V (not 46V as mentioned in document)
- Why am I getting different Voltage output for Lab 2?
- Does the preloaded / already existing coefficients of Lab 2 Compensation designer are for stable system?
In the Compensation Designer, tool is showing unstable system with already modelled coefficients. I was expecting it to be already stable for this design.
Regards,