Dear Team,
Where can I find the specification of the inductor L7 PQ20/20/14-1, Ferrite, 10 uH, 15 A, TH?
Thank you in advance!
Kind regards, Lars
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Where can I find the specification of the inductor L7 PQ20/20/14-1, Ferrite, 10 uH, 15 A, TH?
Thank you in advance!
Kind regards, Lars
Hi Lars,
The details about L7 construction are shown in the design guide of the PMP8740, available at the following link:
https://www.ti.com/lit/pdf/slup348
Please go to page 21 of this guide, where L7 (referred as "Ls") should be built on PQ20/20 core + bobbin, by winding 10 turns of LITZ wire (important to use multi-filar wire because of the high RMS current) made of 160 x 0.1mm strands, while the core should have N97 material. Then add an air gap of 0.77 mm to the core (which corresponds to a ue of 57). By doing that, I calculated copper loss to be 0.63W, while core loss should be 0.57W.
Regards,
Roberto