This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010210: The purpose of the delay

Part Number: TIDA-010210

Dear Sir/Madam,

I saw that there are 6 relays of G4A-1A-PE DC12, i.e., K1, ... K6. My questions are:

  1. Are these relays really necessary because the GaN switches does not have a body diode (No passive rectification)?
  2. Can we only use 3 relays if they are really needed?

Thanks a lot.

  • Hi,

    • GaN has the third quadrant behavior which allows you to have the precharging.
    • By using 6 relays you can have a direct disconnection between the input AC and the output DC.
    • Yes, you can use three relays too.

    Thanks

    Best Regards

    Riccardo