I am using PSPICE for TI to simulate a preamplifier based on TL074. When I add the op-amps to the schematic, each unit appears as a separate IC. How can I make PSPICE realize that all 4 units belong to the same package, and need only one pair of connections to DC power?
P.S. I chose "I don't have a part number" above because this is not a part-specific question and, if I supply the part number, I can no longer select the appropriate forum.