Other Parts Discussed in Thread: LM5180
Hi,
We have a customer whose requirements are similar to TIDA-010006, below are their requirements.
Input: DC20V +/-10%
Output 1: DC20V/120mA.
Output 2/3/:DC15V/50mA each of them.
Output 5/6: DC3.3V/30mA each of them, will have LDO to regulate to have 3.3VDC.
Do we need feedback? will the feedback create cross regulation issue?
Could you help to design the transformer and related circuit for the customer?
Regards
Hely