This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00066: TIDA-00066

Part Number: TIDA-00066

Hello.

I have following requirements for analog amplifier 

Input voltage 1V(rms)
output voltage 300Vpp
Max current 6Apeak
Suitable for a minimum real load of 25 Ohm
Bandwidth (-3dBV): 1kHz to 2MHz

Duty cycle <10

Can you recommend some other reference design or some modification in TIDA-00066 reference design to achieve require results. Thanks

Best Regards

Farhan