Part Number: TIDA-01606
Other Parts Discussed in Thread: UNIFLASH, TMS320F28379D
When I tried to build in 28379d using TIDA-01606, I got the below error.
Do you know what is the problem?
By the way, I can build using TI evaluation card....
Error in build step #3 (Make): Make process exited with code 2:
copy /Y "D:\Ti\tsp_ti_c2000\templates\uniflash\ControlCard_TMS320F28379D.ccxml" ".\output_TI2837xS_cpu1\ForLowVoltageTest.ccxml"
1�� ������ �����Ǿ����ϴ�.
"C:/ti/uniflash_8.2.0/dslite.bat" --flash --config=.\output_TI2837xS_cpu1\ForLowVoltageTest.ccxml .\output_TI2837xS_cpu1\ForLowVoltageTest.out -u
Executing the following command:
> "C:\ti\uniflash_8.2.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\DSLite" flash --flash --config=.\output_TI2837xS_cpu1\ForLowVoltageTest.ccxml .\output_TI2837xS_cpu1\ForLowVoltageTest.out -u
For more details and examples, please refer to the UniFlash Quick Start guide.
fatal: IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.10.0.00080)
ForLowVoltageTest.mk:157: recipe for target 'download' failed
Failed: Operation was aborted
make: *** [download] Error 1