Other Parts Discussed in Thread: LM5160, TPS54560, PMP22343
Hi team,
I would like to adopt this design; however, some components are seems to be a little old.
Especially, the coupling inductor, TA7848-AE, is very difficult to find in the market.
I assume 1:1.05 ratio on this inductor is to take Vf drop on the Positive +15 V side's diode's Vf.
Would there be another alternative for this inductor? What are the parameter consideration for choosing this inductor? (The only changes i would like to have compared to design is +-15 -> +-16V to have 1V drop LDO after this.)
Also, is there a newer IC recommendation for similar application (Fly-Buck)? LM5160 seems a bit old.
Thanks,
Luke