With respect to the TIDM-BPM (Ultra Low Power Blood Pressure And Heart Rate Monitor Reference Design)
- What are the dimensions of the DC air valve?
- What is the MPN of the DC air valve?
- Is there any reference model for the DC air valve which can be referred?
- What is the dimensions of the BP300UF IC and MPN?
- Is the BP300UF IC actually required? or the system can work without it being mounted as well?