Part Number: TIDA-01464
Other Parts Discussed in Thread: UCC28740, TL431,
Hi, please see attached pdf document of the power supply based on the reference design TIDA-01-01464. The values for the Lm and turns ratios as shown for 85-256Vac input
The power supply do not operate correctly, the Vdd shows the ramp error voltage and restarts continuously. There is no three pulses as mentioned in the notes, instead there is a single pulse from the DRV output of the UCC28740. The waveforms on the AUX, and the Secondary are correct. Since there is not enough time for the secondary voltage to rise and provide feedback, the device keep restarting. even with lowering the capacitor value on the Vdd pin from 10uf to 1uf do not provide much benefit. The feedback tested by itself and works correctly by back signal injection to the output.
The Resistor RS1, and RS2 are set fo 77K, and 20K. The value of the current sense resistor has been lowered without improvement.
Another step taken as to examine another similar reference design TIDUAN0B which is for 100W 24V. An identical transformer from Wurth was used, with exact components including using the TL431 feedback as was used in the reference design. Except our project utilizes two switch. Basically the design is identical to the 100Watt, except we uses two switch flyback, Nothing else is different. The problem remains.
Many people are working on this project, and it is affecting the staff in very negative way, please after review contact us immediately. If need additional data please contact. Thanks