Part Number: TIDA-00779
Other Parts Discussed in Thread: UCC28180EVM-573
Hi TI Expert,
Can you let us know how you calculated these 0.2s switch delays using which RC Values in the Design ?
Also, what is the importance of having 2 signal PFC ON and a rectifier(from 2 Diode) signal to turn on MOSFET by which Relay is triggered? Also, a Zener in Series will drop the voltage by 12V, but the MOSFET we select will turn ON at 1-2V only. Then how is the time calculated as 0.2s?
Please explain the given circuit with the equations and how it works.
Also, if we do not want to use the boost follower circuit, then we have to use or consider the divider given in the image below for PFC Boost Circuit.
Waiting for your reply!
Thanks & Regards,
Meet Devendra Pandya