As I understand, the reference design has been tested according to UL217 and is compliant with the sensitivity requirements from this standard.
I am working with a project where the sensitivity requirement is 0,001dB/m, averaged over a period of 5 seconds.
Will the reference design fulfill this requirement? As seen from the design guide and the test-report, the obscuration is measured in "%/ft".
I am not familiar with the "%/ft" to "dB/m" convertion.
If the reference design doesn't fulfill this requirement, are there any changes we may do to improve the sensitivity?
BR Per