Part Number: PMP9802
Other Parts Discussed in Thread: TPS61089, TLV62130, BQ25170
Hi,
I need to design a circuit that looks similar to the one in PMP9802. I have, hence, been studying the material and how the design works and have a question regarding its functionality. As far as I understand, the whole concept is based on the fact that both the TLV62130 and TPS61089 work at power save mode, therefore their outputs can be combined directly, changing at the same time their output nominal values accordingly.
At some point in the test report (section 2.1) it is mentioned that "When the voltage in their VOUT pin is higher than the setting voltage, the TLV62130 and TPS61089 stop switching. No reverse current is flowing into the converters. Using the principle of PSM, the operation sequence of the TLV62130 and TPS61089 can be implemented by setting a different target output voltage." The sentence highlighted in bold by me puzzles me a little bit. I do understand it for the TPS61089 converter, but looking into the SW pin of TLV62130 we have a path through the body diode of the HS-MOSFET towards pin PVIN, isn't there?
Why then do we say that there is no reverse current flowing? Is it because of the external diodes D1 and D2?
In my case, there will only be VGRID at the input of TLV62130 (and not the battery), so if it is missing, won't there be problems because the VBUS voltage is now fed to the input through the path I described above, causing the TLV62130 to startup and switch? I guess I shouldn't rely only on the fact that the converter is turned-off due to VGRID missing, but due to the above effect I should also make sure its programmed output is lower than TPS61089, so as to ensure it stops operation (as in the reference design).
Moreover, when the TPS61089 converter is not switching, is there any current leaking from the supercap towards the converter and its output? I'm only asking this because in my case, the supercap is in reality a Li-Ion battery and I'm worried that its charger (bq25170) will not be able to terminate the charging cycle within the 10-h window due to current leaking from the battery towards the TPS61089 and VBUS.