This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSPICE for TI ERROR(ORPSIM-16583): when running circuit .op (dc bias) command

Hello,

In PSPICE for TI, I'm getting a "ERROR(ORPSIM-16583): More than one imported model containing transistors or diodes is detected. To simulate this circuit, a minimum of 1 and a maximum of 4 traces are required. Reduce the number of traces and simulate again." error when doing a dc bias/.op simulation.  I have multiple non-TI op amps in the circuit if that is relevant.  I'm only asking for voltage and current outputs.  I switched the power & noise outputs off.  Any ideas how I can fix this?

Thanks.