Other Parts Discussed in Thread: SN65HVD1786, THVD8000
Hi All,
I have created a project based on this:

The device on the left in the transmitter, the right one is the receiver.
On the left device: DE and REZ are connected to +5V and R is left open, on the right device DE and REZ are connected to ground and D is left open.
Supplied power to the left coil is 12V. The rest of the schematic is the same.
When nothing is connected at the right coil, the signals on A and B are:
Red is signal A, signal B is green. The right device gets power from a separate power supply.
First question: is it possible to reduce the spikes in both signals?
But when at the right coil a LM7805 is connected which will supply power to the right device, the signals become:
The blue signal is the data received and is correct, but signals A and B are very disturbed.
Is it possible to maintain a steady signal on A and B?
The cable length is 1 meter.
I hope someone can help me.
Thanks is advance.