Part Number: LP-XDS110
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1, ENERGYTRACE
Hi.
My system: Ubuntu 22.04 kernel 6.5 / CCS 11.2 or 12.7 / SDK 6.10.0.29 / LAUNCHXL-CC26X2R1
Just running ProjectZero. I've trying to use the EnergyTrace but it does't work on Linux. It starts measuring for some seconds and hangs, sometimes doesn't start. I've tried the target with JTAG, cJTAG 2 and 4 wires. It seems with JTAG is a little better.
The following messages used to appear:
- Cortex_M4_0: JTAG Communication Error: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.7.0.00213)
- IcePick_C: Error: (Error -261 @ 0xFFFFFEFB) Invalid response was received from the XDS110. (Emulation package 9.7.0.00213)
But I tested the same project on a VirtualBox Windows 10 machine, running on the same computer and Linux, CCS11.2 and SDK 6.10.0.29, and the EnergyTrace runs flawless w/o any error.
Any tip?
Thanks
Marco