Other Parts Discussed in Thread: LM5171, , TPS55288EVM-045
I would like to replace the Enphase Microinverter with your new GAN Microinverter
TIDA-010933
1.6kW, bidirectional micro inverter based on GaN reference design
I would like to combine the LM5171 or comparable at either 3 or 6 volts with this your new GAN Microinverter so when the sun goes down and the solar stops working we can discharge the 600 watt 3-6 volt dc batteries to AC Grid. The issue is the TIDA-010933 only goes down to 25 volts so we need a way to step up the voltage of the battery from 3-6 volts to 25 volts so TISA-010933 can send this dc to ac grid! The reason I want to stay at 3 volts is that its a 600 watt 3 volt cell then we. That way we dont need to balance or bleed the cells or use a BMS. Im open to 3 or 6 volts for the battery voltage but prefer 3 volts.