This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5045: LM5045

Part Number: LM5045


The LM5045.Lib model LM5045.LIBLM5054_LLC-Bridge_SiR668-MOSFETs_v02.TSCdoes not show any clock in the Tina TI- Simulation. The rising edge of the of the input voltage step was 100µs for 0V to 24V.

Do you have any idea to solve the problem?.

  • Need more explanation please? "Rising edge of input voltage step?" "Does not show a clock?" LLC Bridge requires variable frequency but LM5045 is a fixed frequency controller. Please explain what you are trying to achieve and what the perceived problem seems to be? Why is COMP pin and SR1/SR2 floating - is this intentional?

    Regards,

    Steve