This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01495: U10 correct part?

Part Number: TIDA-01495

Hi there, I've been working through this design. Could you advise if U10 is the correct part, it is listed as a 78L05, 5v regulator but has an output netlist named IOS_15v. It also appears from the datasheets that the destinations of that netlist flag would be looking for 15v and not 5v; this would be U7, U8 (UA78L15ACD) and Q6 which is being used to generate 5v. Could it be that U10 should be a 78L15 instead?

Thanks

Ryan