This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-020047: LM62460-Q1 Not working

Part Number: TIDA-020047
Other Parts Discussed in Thread: LM62460-Q1

Hello ,

I'm trying to understand why the LM62460-Q1 preregulator isn't functioning properly. When I measured the voltage at R217, which is connected to the PRE_REG_PG pin, I found it to be 0V. Could this indicate a fault with the preregulator? Should I consider replacing it to resolve the issue?

PS: I'm working on TIDA020047 board.

 

Regards

Amine.