Part Number: PMP23340UCD
Other Parts Discussed in Thread: UCD3138A
Hi,
Thank u for ur time.
I have some doubts about PMP23340UCD.
Hardware:PMP23340UCD(UCD3138A)
Firmware:TI supplied routines——UCDIBCFirmware
Issues:
- The PMP23340UCD is referred to as open loop in the documentation, does this mean that the FE, Filter are not involved in the operation?(both EAP0 and EAP1 have inputs on the schematic)
- If it is open loop,what does the YN depend on ?
- What does PID_PERIOD_FACTOR mean?
- With the same VIN and load, adjusting the frequency, the VOUT change is not significant because the Gain change is small?(The dpwm output waveform is consistent with the adjusted frequency).
- Is Automatic Mode working in open loop and what mode is the PWM in at that time? Does changing the frequency_switch change the PWM mode?

Best Regards.