Part Number: PMP23340UCD
Other Parts Discussed in Thread: UCD3138A
Hi,
Thank u for ur time.
I have some doubts about PMP23340UCD.
Hardware:PMP23340UCD(UCD3138A)
Firmware:TI supplied routines——UCDIBCFirmware
Issues:
- I found that the frequency_switch is adjusted through the GUI and eventually written to pmbus_dcdc_config[0].min_period.And then how does the firmware reconfigure the DPWM module output frequency? (I didn't find the correlation logic for this, and didn't notice configure_dpwm_timing() being called after this)
- The GUI can only set frequency_switch within (1±20%) 1000KHZ, is it because the Filter output camp is limited?
- I found that the limiting issue is related to the following two functions, but I can't read the period_change() function, it doesn't seem to change the filter limit value?
- After adjusting the frequency through the GUI, where does it determine if the threshold is exceeded (if it's at the filter output, why go through the filter just to change the frequency)?



Best Regards.