Part Number: UCC28180
Hi,
I'm running the PSpice model in file SLUM423.ZIP provided for UCC28180. I would like to know what is the value of default voltage - 162V referring to? Based on the design calculator provided in excel file SLUC506, i guess this 162V is the conversion value from RMS input voltage to average voltage, but not sure which value is this referring to.

Also, I'm quite new with pspice, i need some guidance on the simulation profile as the default simulation profile is run under AC Swipe/Noise. When i edit the simulation profile to time domain, and set the run time to 1000ms, i observed that the Vload is decreasing (not 390V).

And same goes for the output current. 
Kindly advice, thank you.
Baz