Part Number: TIDA-050063
Other Parts Discussed in Thread: TPSI3052-Q1,
Tool/software:
Hello,
I have noticed in the refernce design that the current amplitude is rather consistent trough the precharge cycle but there is a small slope on it. (see the red line in the picture below from the reference design, Figure 3-4).
In my application, I need to reduce the inductor size and therefore have a much smaller saturation current and consequently a lower current swing. I have therefore decided to use 2.5A as my upper limit and 0.5A as my lower for the target value in the feedback loop. It seems that the lower the inductance the more aggressive the angle of that slope gets. In my simulations it now looks like I'm getting quite a lot of negative current spikes (charging the battery). (~400mA). 
This doesn't seem realistic to me and I don't know what implications it would have. Could you please shine some light on:
-Where does this slope come from?
-What are the implications of the negative charge current?
I attached the graphs from the simulation and a picture of my simulation setup. Let me know if you need anything else.
Best,
Emil
plot1 (1).pdf