Other Parts Discussed in Thread: PMP23340UCD, UCD3138A
Hi,
Thank u for ur time.I have some doubts about PMP23340UCD.
Hardware:PMP23340UCD(UCD3138A) (48v-12v)
Firmware:TI supplied routines——UCDIBCFirmware
When the board is working in resonant mode, I want to modify the phase shift of DPWM0 and DPWM2 on the primary side, via the GUI.
- In the init_dpwm2() function, change the INTRA_MUX in resonant mode from BELOW to CROSSOVER.But the board works intermittently.What is it about?


- I'm guessing the following code is causing the board to work intermittently,after the modification, DPWM2 at resonance is not in phase with DPWM0, correct?
- What does this code do?

- Modified in the main function, the board works fine, but why is the current getting higher? Is it because there is still a phase difference?
- How do I properly implement the phase shift control of DPWM0 and DPWM2?


Regards,
Martin.