Part Number: TIDA-010054
Other Parts Discussed in Thread: TIDM-02000
Tool/software:
In reference to the TIDA-010054 Dual Active Bridge design...
It's my understanding that as of roughly 4 years ago, Peak Current Mode Control had not yet been implemented, hence the need for the DC blocking capacitors in the design. Is this still the case or has this control been implemented? If it has, is there a reference that exists to understand its implementation? In the design guide TIDM-02000, PCMC is implemented for a PSFB converter, is this applicable to a DAB converter as well?
Further, in a high power Dual Active Bridge design with a large voltage conversion ratio, the secondary transformer RMS currents are significant enough that the implementation of the DC blocking capacitors becomes challenging. Are there intricacies involved with PCMC that preclude it from being used in such a design? If so, are DC blocking capacitors the only effective way of preventing transformer saturation?
Thanks