Other Parts Discussed in Thread: TIDA-010062, PMP41006, PMP41037
Tool/software:
please share details of YXS61041T make YAXIN ELECTRONIC TECH. it is not available on interent.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I used this one in the last version, please refer.
Hello Desheng,
This transformer is used in PMP4103 - 1kw 800 to 12V active half bridge topology. In BOM transformer part number is YXS61041T. Part suggested by you is inductor . Please share details of YXS61041T.
Regards,
Sandip
PMP4103
Hi Sandip,
I used YXS61075T in PMP41081, YXS61041T is used in TIDA-010062 and PMP41006.
YXS61041T is dedicated for LLC, it included SR FET and capacitors on the secondary PCB winding, you may need remove all the capacitors, if you want to use it in PSFB.
Are you talking about PMP41081? I believe I designed it with 400V to 12V.
For 800V input, you may refer to PMP41037.