This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01179: Zener used in VCCX Bias Supply Path

Part Number: TIDA-01179

Tool/software:

Hello, is the Zener diode (D7) used in the bias supply path for VCCX correct? The voltage applied to the VCCX pin must never exceed 15 V, however, the zener voltage of D7 is 12 V.

The output voltage of the reference design is 15V, that means the Zener diode is conductive. Two 300 Ohm resistors in parallel (R16 and R11) limit the current to 100 mA (15 V / 150 Ohm). 

Power dissipated over D7 = 100 mA * 12 V = 1.2 W

Zener diode used: BZT52C12T-7

  • Max Pd = 300mW

1.2 W > 300 mW -> Zener diode goes up in flames.

Where am I wrong?

 

  • Found my error, I assumed that the voltage over R16 and R11 is 15V, which is obviously not the case. It is 3V (15V - 12V = 3V). That means the current through D7 is 20mA max. 

    Pd = 20mA * 12V = 0.24 W

    All good.