Part Number: PMP23404
Other Parts Discussed in Thread: LM5143-Q1
Tool/software:
hi Sir
May I know why the SW1 is empty pin?
thanks

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This SW1 pin is actually connected to Q3 drain / Q1 source in actual layout. The PMP23404 also incorrectly shows Vout (middle right edge of schematic) to be 3.3V, when it is actually 5V. On the other hand, the correct connection of U1 pin 28 FB1 to ground is shown to set Vout at 5V.
You point out my second question, FB1 connected to VDDA by R16, 0 ohm to generate Vout1 in 3.3VDC and FB2 connected to GND to generate Vout2 in 5VDC. How could TI come out the test report by a reference design connected Vout1 & Vout2 together in different output voltage?
Hi Alex, thanks for catching these, the schematic will need to be updated. SW should be connected to the output filter. The picture you inserted above is slightly different than the schematic in the PMP23404. Both FB is connected to GND for 5V output.
https://www.ti.com/lit/df/tidmby8/tidmby8.pdf?ts=1719414916141
With single output 2-phase with the LM5143-Q1 Mode is always tied to VDDA and FB2 to ground:
From the LM5143-Q1 datasheet: