Tool/software:
Hi Experts,
I have recently started using the TIDA-00254 reference design. I have a Lightcrafter 4500, a Basler a2A1920-160umBAS USB 3.0 camera, and all the associated cables. The Basler ace is capable of being hardware triggered, so I assembled the trigger cable to connect the Lightcrafter to the camera like the reference design described.
In the DLP Lightcrafter 4500 config.txt file, I have set CAMERA_TYPE = 0 like the reference design describes for an Open CV camera. In the config_camera.txt file, I have set these parameters:
# Rolling shutter color Camera - MONO8
# Global shutter Monochrome camera - RAW8
When starting the scanner application, it says both the Lightcrafter and the camera have connected. The issue is, my Basler USB 3.0 camera is not connecting. Instead, my computer webcam is connecting. I am not sure why this is occurring and I do not know how to fix it.
If anyone could provide support on how to connect my Basler ace camera to this application instead, that would be greatly appreciated. Please let me know if I can provide any additional information.
Regards,
Josel