Part Number: TIDA-010208
Other Parts Discussed in Thread: CSD18536KCS, TIDA-010247, BQ76952, BQ76942
Tool/software:
Hi,
If the high-side driver MOSFET circuit from TIDA-010208 was placed on a PCB with much thicker tracks (like 1.5mm copper sheet) could these two sets of three MOSFETs safely handle a 200A load? What if all 6 main MOSFEETs were replaced by CSD18536KCS (in TO-220 package) as they would be easier to fix?
What changes would be needed to each of the gate driver circuits to drive six MOSFETs in parallel?
Many thanks,
Ian