Part Number: TIDA-010933
Tool/software:
Hi Expert,
I have some questions about the sample code of TIDA-010933:
1. uINV_DCAC_runISR1_lab3

Why does the final result output need to be *-1? So it feels like the output becomes the opposite?
In addition, what is the purpose of passing the DC voltage through the band rejection filter?
2. uINV_DCAC_runISR1_lab4
uINV_DCAC_runISR1_lab5
Why do we need pr to control the 1st, 3rd, 5th, 7th and 9th harmonics?
3. void computeDF22_NotchFltrCoeff(DCL_DF22 *v, float32_t Fs, float32_t notch_freq, float32_t c1, float32_t c2)
What do the c1 and c2 parameters of the band rejection filter represent?
4. Which method do we use for z conversion in the programming of pr controller and band rejection filter?

Best Regards,
Seamus