Part Number: TIDA-01487
Other Parts Discussed in Thread: TCAN1042HG, SN74LVC2G132, SN74LV132A
Tool/software:
Hi team,
Based on TIDA-01487, the attachment is the schematic design of a non isolated CAN relay that customers have modified.
The current debugging situation is that after connecting communication devices to TCAN1042HG, the buses on both sides are usually set to a fixed level after a short period of CAN message waveform. The capacitor C6 C8 and resistor R6 R7 in the delay section were attempted to be modified to 4.42k and 47pF, which are consistent with the reference design, but still cannot work properly.
Could you kindly help analyze the possible reasons and provide suggestions for us?
Thank you!
Regards,
Maggie