This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP4408: SMPS FLYBACK

Part Number: PMP4408


Tool/software:

Hi sir,

   

We need to design an SMPS Flyback topology with the following specifications:

Input Voltage: MAX 275VAC

Output 1: 12V 5A

Output 2: 5V 5A

Please recommend a suitable transformer and control IC for this design.