Part Number: TIDA-010933
Other Parts Discussed in Thread: LMG2100R044, LM5164
Tool/software:
Hello,
We are going to design our own micro Inverter and we are refering the TIDA-010933 reference design for this purpose.
We have go through the reference schematic and there are some questions as mentioned below,
1) Should we follow the same schematic provided in TIDMCF8A.ZIP for our own design?
2) In our design, there is only the Input from the PV to the design, we are not going to charge the 48V battery OR power from 48V battery. As I have seen the U1_A, U1_B, U1_C, U1_D (LMG2100R044) pin#5 (sw) is connected to the PV voltage input and Pin#7(VIN) is connected to the vout. So this true for our application? Please find the below image for your reference.

Where as the same IC LMG2100R044 is used in next stage which has the corrent connections look like, below is the reference Image,

3) Do we need to add any Induction at the sw pin of either U7 or U9 for LLC resonant? Below is the reference Image.

4) Initially, when we connect the EVM to PV at that time, MCU and other devices need the 5V and 3.3V so how it will be there on board, So kindly guide us the power topology at power ON and then after.
5)The MPPT stage needs to generate 75VDC as output. But the P&O algorithm will adjust the voltage to maintain the Point at Max Power, then how can it maintain the O/p voltage to 75VDC all the time?
Regards,
Alpesh