Tool/software:
Greetings,
We wanted to use your arbitrary logic in our design. We copied everything, even the same components(not intended). Where we found the issue to be, is in communication between isolated and nonisolated CAN networks. When we want to transfer information from one side to the other we have no problem, doesnt matter the side, but when we want those two side to communicate it looks like our isolated CAN side cant get the message trough. Our device on isolated side can send only one message before getting, we are guessing, blocked by other messages on nonisolated side. Nonisolated side continues to communicate with zero issues and messages are sent every 100ms (CAN is opperating at 500kb/s), which is not enough to clog the network in our opinion.
Arbitrary circuit is on the nonisolated side of the CAN network. What we did differently is instead using the isolated power supply that you suggested, we have put TEL6-1212, and than trough LDO we are dropping it to 5V and one more thing, except using your TCAN1042 we are using NXP PCA82C250. Everything else is the same.
Is it possible that you encountered similar problems while testing yours design?
Your help is much appreciated
Thank you in advance
Best regards,
Stefan