Tool/software:
Hello dear, I would like to know if the resonant inductor YXS50494T used in the scheme is coupled, being a single inductor coupled for the two phases, or each phase has a single inductor?
Would it be possible to obtain the technical specifications of this inductor used in the reference design?
And I would like to know if there is any report or measurement of the temperature of the reference design in thermal regime in 3 kW operation.
Thank you very much for the help and information.