Tool/software:
Hello there,
I have been simulating using the model provided here
However, the SS pin doesn't appear functional?
When Vss drops to 0, due to hitting I limit, the switches keep switching unabated as if nothing happened.
Is the model incomplete?
There is an undocumented subckt parameter, SS, which shows the same behavior when set to 0, or 1
I also tested the model that was exported from WeBench, with the same result: SS doesn't influence the switches.